Abort
Closes one or more graphic displays. Without a parameter, the
Abort
command closes the window that has focus.Syntax
Abort [
parameter
]
where
[parameter]
is one of the following:- Mecloses the graphic display from which the command is issued
- display_namespecifies the graphic display to be closed. This can be a relative or absolute reference to a graphic display
- *closes all visible graphic displays. Cached displays are also closed but not removed from the cache.
- /Dused with the * (close all) parameter to specify that all docked displays and the navigation menu be closed as well. If this parameter is not used, when the Abort* command is issued, any docked displays and the navigation menu will remain open.
Remarks
The command syntax
Abort Me
does not work when issued from within in a macro file. When issued from a graphic display, the graphic subsystem supplies the name of the current display in place of Me
to the command subsystem. However, when a command is issued from a macro this does not happen.This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.Provide Feedback