AppAbort
Closes the specified Windows application.
Syntax
AppAbort <
program
>
where
<program>
is the name of the program. This should be exactly what is displayed in the title bar of the application.AppAbort Untitled - Notepad
Remarks
This command is run locally on the HMI server,
FactoryTalk View SE
Client, or FactoryTalk View Studio
that issued it.Provide Feedback