AppActivate
Activates the specified Windows application by bringing the window to the front. The program must already be running. (You can use the AppStart command to start the program.)
Syntax
AppActivate <
program
>
where
<program>
is the name of the program. This should be exactly what is displayed in the title bar of the application.Remarks
This command is run locally on the HMI server,
FactoryTalk View SE
Client, or FactoryTalk View Studio
that issued it.When you activate a program using AppActivate,
it is opened behind the main FactoryTalk View window. This is a result of certain operating system rules. You can either manually give focus to the program or you can work around this programmatically. For information on the workaround, see Knowledgebase Document ID: BF15995 - Use Windows to Move External Application Window to Foreground.
Provide Feedback