FlushCache

Without the parameter,
FlushCache
unloads all graphic displays from the display cache. With the parameter,
FlushCache
unloads the specified graphic display from the display cache.
Displays can be added to the cache by using the /Z or /ZA parameter with the Display command or by selecting the Cache After Displaying option in the Display Settings dialog box of the Graphic Display editor. You can cache up to 40 graphic displays.
Syntax
FlushCache [
component
]
where
[component]
is a relative or absolute reference to a graphic display. If the file name has a space in it, enclose the name in double quotes.
Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a
FactoryTalk View Studio
or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal