Using a parameter list

You can use a parameter list, instead of a parameter file, to provide tag or folder names, or parts of tag names, to the tag placeholder in a display list selector object at runtime. This lets you to use different sets of tags with a single display list selector.
The advantage of using a parameter list, over using a parameter file, is that the parameter list stays with the object and is moved and copied as the object is moved and copied.
A parameter list is particularly useful with the faceplates, which tend to come in groups with secondary displays opening from a primary display. You can also assign just a folder name in the primary display, which, when carried forward into a secondary display, defines a structured tag. When a secondary display opens, it automatically applies the appropriate tags from the folder to the display objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal