Using a parameter file
You can use a parameter file with a graphic display by specifying
/P
after the name of the graphic when you give the Display
command. The syntax is:Display <graphic file name> /P<parameter file name>
You can also use a parameter file with a display list selector object, by selecting the
Parameter file
option in the States
tab and specifying the name of the parameter file.
TIP:
If the parameter file name contains spaces, it must be enclosed in double quotes.
Provide Feedback