Create a parameter list
You can define a parameter list in the
Display List Selector
object so that the tags will be used by the display that is specified for the state.
TIP:
The first tag in the list will replace #1 in the display expressions, the second tag in the list will replace #2, and so on.
To create a parameter list:
- In FactoryTalk View Studio, on a display, right-click theDisplay List Selectorobject and selectProperties.
- In theStatestab, select theParameter listoption of a state and click theBrowsebutton.
- In theTag Browserdialog box, select a tag and clickOK.
- To add more tags, repeat steps 2 and 3.
Provide Feedback