Select multiple graphic objects

After you have selected a number of objects, you can click in the drawing area away from any objects to deselect them. You can also make them into a group by selecting
Arrange
>
Group
.
To select more than one object, do any of the following:
  • Select the first object, then press
    Ctrl
    and then click to add the object to the selected group.
  • Place the pointer above the objects and drag diagonally to create a selection border around the objects. When all the objects are inside the border, release the mouse button. The border is replaced by handles on all selected objects. You can add objects to this group by pressing
    Ctrl
    and clicking them.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal