Edit the links for an embedded object
Use the
Links
option on the Edit
menu to edit the links for the selected linked object. The list box shows the source application, type, and update option specified for the selected object.To edit the links of an embedded, linked object:
- InFactoryTalk View Studio, in theGraphicseditor, select the object and selectEdit>Link.
- In theLinksdialog box, make the required changes to the objects links. If the object has multiple links, click one to edit it.
- When you have completed the changes, clickCloseto save them and exit.
Provide Feedback