Change the icon for an OLE object
You can use the
Change Icon
dialog box to change the icon to represent the OLE object you have selected to insert.To change the icon for an OLE object:
- In theInsert Objectdialog box, select theDisplay as Iconcheck box and then clickChange Icon.
- In theChange Icondialog box, selectCurrent,Default, orFrom Fileto indicate which you intend to use as an icon.
- If you selectFrom File, click the browse button(...)to locate and select an icon.
- ClickOKto return to theInsert Objectdialog box.
Provide Feedback