Draw a freehand object

You can use the
Freehand
option on the
Objects
menu to draw shapes as you would with a pen on paper. A freehand object is not restricted to the grid even if the grid is on.
To draw a freehand object:
  1. In
    FactoryTalk View Studio
    , in the
    Graphics
    editor, select
    Objects > Drawing > Freehand
    .
  2. Drag the tool to create the shape you want.
  3. In the
    Freehand Properties
    dialog box, change the styles if needed. If you have chosen a fill pattern, the object is filled as accurately as possible even if it is not a closed figure.
  4. When the object is complete, draw another object. You can also click to finish drawing with the tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal