Import an image

Use the
Add Component into Project
dialog box to import an image to the
Images
folder.
TIP:
When importing a JPG, PNG, or SVG graphic image, the image file extension is changed to .bmp, but the file type remains what the original image is.
FactoryTalk View
installs a set of commonly used PNG images in C:\Users\Public\Documents\RSView Enterprise\Images\Rockwell Library Images. Import them to the
Images
folder to simplify your application development.
To import an image to the Images folder:
  1. In the
    Graphics
    folder, right-click
    Images
    and then select
    Add Component into Project.
  2. In the
    Files of type
    box, select the type of image to add.
  3. Navigate to the directory where the .bmp, .png, .jpg, or .svg file is stored, and then click the file name.
    Shift-click or Ctrl-click to select additional files.
  4. Click
    Open
    to add the selected files to the list in the
    Images
    folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal