Add a Symbol Factory image

Use the
Image Browser
to add an image from Symbol Factory to a graphic object.
To add an image from Symbol Factory to a graphic object using the Image Browser:
  1. In the graphic display, draw the graphic object you are going to import an image for.
  2. In the
    Image Browser
    , click
    Launch Library...
    .
  3. Browse the
    Categories
    frame, and select the graphic to be used.
  4. Click
    Copy as,
    the Symbol Factory minimizes, returning to the
    Image Browser
    .
  5. Click
    Paste from Library
    .
  6. Type a unique name for the image, and then click
    OK
    .
    The graphic will now be displayed in the Preview window. The graphic has been added to the list in the
    Image Browser
    . This also adds the image to the
    Images
    folder in the
    Explorer
    window.
  7. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal