E-Signature tab of Properties dialog box

Use the
E-Signature
tab of a graphic object's
Properties
dialog box to configure the electronic signature capability to control and record operator actions.
The following graphic objects have the common
E-Signature
tab options:
  • Push Button
    • Maintained Button
    • Latched Button
    • Multistate Button
    • Interlocked Button
    • Ramp Button
  • Advanced
    • Control List Selector
    • Piloted Control List Selector
The following table shows the options on the
E-Signature
tab.
Options
Description
Require E-Signature
Turns on the electronic signature function to control and record operator actions.
Allow blank comment
Allows empty comments when the operator or approver executes the action.
Show confirmation message
Shows a confirmation message when the operator or approver executes the action.
Select this check box, and then edit the confirmation message.
Insert Variable
Inserts a type of variable to the confirmation message. After you set up the embedded variable, the syntax appears in the confirmation text box. At runtime, it will be read as part of the confirmation message.
Require re-authentication
Requires the password when the operator executes the action.
Require counter signature
Requires the authentication by another person to execute the action.
Authorized Group
Lists all the groups in FactoryTalk Security. All members of the selected group can be a supervisor of this object.
You do not need to add the Authorized Group to Runtime Security.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal