Configure general properties of a piloted control list selector
After you set up the options in the
General
tab, click the States
tab to specify how the selector looks in each state at runtime.To configure general properties of a piloted control list selector:
- In thePiloted Control List Selector Propertiesdialog box, in theGeneraltab, specify the following properties if needed:
- general appearance for the selector list and its text
- number of states
- when the value for the selected state will be written out
- whether the user can navigate to the piloted control list selector and give it input focus using the keyboard
- whether the list will wrap when scrolling
- ClickOK.
Provide Feedback