Create an arrow object
An arrow object can move vertically or horizontally based on the results of an expression. The rectangle you draw when you create an arrow defines the arrow's path. The orientation of the rectangle (vertical or horizontal) should be the same as the direction the arrow is to move in.
To create an arrow object:
- In theGraphicseditor, selectObjects>Advanced>Arrow.
- Drag the mouse to draw a horizontal or vertical rectangle that defines the length and orientation of the path the arrow will move along.
- In theArrow Propertiesdialog box, in theGeneraltab, specify the following fields:
- Expression
- Range
- Direction
- In theCommontab, set up how the object will appear at runtime.
Provide Feedback