Set up connections for a multistate push button
Use the
Connections
tab to set up connections.To set up connections:
- In the Graphics editor, in a display, double-click the object to open thePropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to each connection.
TIP:
To provide visual feedback that the
Value
connection has been written to the data source, assign different tags to the Value
and Indicator
connections. Configure the data source to pass the Value
connection’s value to the Indicator connection.Provide Feedback