Multistate Push Button Properties - Connections tab

The following table shows the options in the
Connections
tab of
Multistate Push Button
Properties.
Options
Description
Value
Assign a tag to the Value connection. The Value connection triggers the multistate push button's action.
Indicator
Assign a tag or expression to this connection. The Indicator connection provides visual feedback to the operator about the button's state.
The following table shows the options under
Columns
in the
Connections
tab of
Multistate Push Button
Properties.
Options
Description
Name
This column shows the name of the connection.
Value update direction
This column shows an arrow to indicate which way data can flow between the connection and the data source.
Right arrow symbol.png tag or expression updates the data source (write connection)
Left arrow symbol.png data source updates the tag or expression (read connection)
Double arrow tag or expression updates the data source and data source updates the tag or expression (read-write connection)
Tag/Expression
Type the tag name or expression associated with the connection. If a tag or expression has already been selected, it is displayed here.
Tag button (...)
Click this button to open the Tag Browser and choose a tag instead of typing the tag name in the Tag/Expression column.
Exprn button (...)
Click this button to open the Expression editor and create an expression instead of typing the expression in the Tag/Expression column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal