Set up auto repeat for a multistate push button
If you set up auto repeat, when the operator presses and holds down the button, repeated button presses are registered until the operator releases the button. For each button press, the application sends the new value to the data source.
To set up auto repeat:
- In the Graphics editor, in a display, double-click the object to open thePropertiesdialog box.
- Click theTimingtab.
- Specify the auto repeat settings to use with the button.
Provide Feedback