Multistate Push Button Properties - Timing tab
The following table shows the options of the
Timing
tab of Multistate Push Button
Properties.Options | Description |
---|---|
Auto repeat rate | Select the number of times per second a button press is registered when the button goes into auto repeat mode. Select 0 if you do not want to use auto repeat. |
Auto repeat delay | Select the length of time the button has to be pressed and held down before auto repeat starts. |
Provide Feedback