Reset the port number
By default, the custom website uses port number 49280 and the HTTPS protocol uses port number 443. If port 49280 or 443 is not suitable for your system, for example if it is being used for other purposes, reset the port number.
To rest the port number, you need to configure the Internet Information Services and the policy of FactoryTalk View SE in FactoryTalk Admin Console.
Changing the port number on one HMI server computer does not change it Directory-wide. If you change the port number here, be sure to change it to the same number on each of the HMI server computers.
To reset the port number
- On each HMI server computer, selectStart > Windows System > Control Panel > Administrative Tools > Internet Information Services (IIS) Manager > Sites.
- Right-click the website that you want to change and selectEdit Bindings.
- In theSite Bindingsdialog box, select the row, and then selectEdit.
- In thePorttext box, type the number of the port, and then clickOK.
- In FactoryTalk Administration Console or FactoryTalk View SE, selectSystem > Policies > Product Policies > FactoryTalk View SE, and then double-clickCustom WebsiteorHTTPS Protocol.
- In thePort Numbertext box, type the same port number as in Step 3.
Provide Feedback