Proxy

Proxy connection can be configured through the
Connection Settings
Tool.
NOTE: See FactoryTalk Remote Access Tools for further information on this subject.
You can choose among three proxy types:
  • None:
    No proxy configuration.
  • HTTP:
    The HTTP proxy supports Basic authentication (BA) or no access authentication method.
    NOTE: Other access authentication methods (for example, DIGEST or NTLM) are not supported.
  • SOCKS5:
     The SOCKS5 proxy does not require any authentication method.
    NOTE: No access authentication method is supported.
NOTE: See FactoryTalk Remote Access Manager Tools access and FactoryTalk Remote Access Manager Tools installation for further information on the
Connection Settings
Tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal