FactoryTalk Remote Access
Tools

FactoryTalk Remote Access
Tools consist of a set of software applets for Windows OS, that allow to manage the devices connection. They shall be installed onto the local computer and can be used to carry out several remote tasks, such as remote desktop connection, files transfer, Runtime processes monitoring and information reference, and establishment of a VPN connection with the Runtime installed on the remote device to name a few.
Tools consist of four applets:
  1. Interactive Access:
    It allows to establish and manage a VPN, serial or USB device connection. Furthermore, it provides an overview of the connected devices.
    NOTE: See Interactive Access Tool for further information on this subject.
  2. Device registration:
    It allows to register a new device that you wish to control remotely to a domain.
    NOTE: The
    Add Device Locally
    parameter refers to routers registration only.
  3. Device setup:
    It allows to manage router settings. It discovers any routers and configures their LAN connection.
  4. Connection settings:
    It allows to set the connection port and proxy server type. These settings are used for establishing a VPN connection between the
    FactoryTalk Remote Access Manager
    and the devices registered to the domain.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal