FactoryTalk Remote Access Manager
Tools installation

FactoryTalk Remote Access Manager
might require the installation of the Tools on your local computer to provide specific features.
Access the
FactoryTalk Remote Access Manager
and select
Tools
Download
to download all the Tools.
NOTE: See Tools for further information on this subject.
NOTE: See FactoryTalk Remote Access Tools to learn more information about the Tools.
Tools can be installed on the following operating systems:
  • Windows 10
  • Windows Server 2008, 2008 R2, 2012, 2012 R2, 2016, 2019 and 2022
Once installed, the Tools are ready for use.
NOTE: Whenever you access a Tool that requires update, a message window will appear, asking you whether you want to proceed with downloading its updated version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal