Move a range
Move a range to a different zone.
TIP:
You can also move a device by editing the device properties. See Edit a range.
- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone that contains the range.
- SelectDevices.
- Right-click a range and selectCut.
- Right-click blank space and selectPaste.TIP:You can paste the range to a different zone or to the list of unassigned devices. Switching betweenCanvas,Zones, andDevicesdoes not discard the copied device.InCanvas, you can drag devices between containers. You can also drop ranges from theGraphical Explorertree to theCanvaspolicy model visualization or in the opposite way.IMPORTANT: InCanvas, when you move a range from theOnboarding Areato aZoneor to theUnassignedcontainer, the device cannot be moved to theOnboarding Areacontainer again.
Provide Feedback