Edit a range
Edit the properties of a trusted IP addresses range.
- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone that contains the range.
- SelectDevices.
- Select the range to edit.
- Make changes inRANGE PROPERTIES.For more information, see Range properties.
Provide Feedback