- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Text box
Insert and view a text at runtime
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Text | Text | Text inserted and displayed | |
Text horizontal alignment | TextHorizontalAlignment | Indicates where the text is positioned on the horizontal axis | |
Text vertical alignment | TextVerticalAlignment | Indicates where the text is positioned on the vertical axis | |
Value change behavior | ValueChangeBehaviour | Mode of updating text when the user writes in the text box. At end of typing: update the value after the user has pressed Enter with either physical or virtual keyboard (pressing Esc or clicking outside the object, the previous text is restored); When typing: in real-time when writing | |
Font family | FontFamily | Font family | |
Font weight | FontWeight | Font weight | |
Font italic | FontItalic | Enables/disables italics in the text | |
Font size | FontSize | Font size | |
Text color | TextColor | Color of the text to display | |
Border color | BorderColor | Color of the polygon border | |
Placeholder text | PlaceholderText | Text to display when the box is empty, typically an example or indication for the user | |
Control in read-only mode | ReadOnly | Enables/disables the read-only mode. If enabled, it is not possible to write in the text box but. For example, it is possible to select the existing text for copy-paste | |
Content Type | ContentType | Content type. Normal: characters displayed; Password: characters hidden | |
Style | Style | Graphic style applied to the control | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Events
Provide Feedback