Data grid column

Data grid column

Data grid object column
BrowseName
DataGridColumn
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Title
Title
Panel title, to be displayed in the navigation tab of a Navigation panel object. If not set, the panel BrowseName is displayed
Width
Width
Width of column. Auto resizes columns when the Data grid is resized. Numeric value maintains specified column size when the Data grid is resized
Visible
Visible
Show/hide the window
Header alignment
HeaderAlignment
Horizontal alignment of the content in the header row
Content alignment
ContentAlignment
Horizontal alignment of the content in the rows other than the header row
Order by
OrderBy
Attribute/property of the nodes or column of a table by which to sort the elements. Generally the same attribute/property or column from which the elements are obtained is set
Data item template
DataItemTemplate
Data item template object which can contain data in textual or image format
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal