Function Generator (FGEN)

Supported controllers and firmware revisions
Controller
Firmware revision
CompactLogix
5380
38 and later
Compact GuardLogix
5380
38 and later
GuardLogix
5580
38 and later
ControlLogix
5580
38 and later
ControlLogix
5590
38 and later
CompactLogix
5390
39 and later
The Function Generator (FGEN) instruction converts an input based on a piece-wise linear function.
Available Languages
Ladder Diagram
FGEN LD instruction linear function
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
Ladder Diagram
Operand
Type
Format
Description
FGEN tag
FUNCTION_
GENERATOR
structure
FGEN structure
In
REAL
tag / immediate
The analog signal input to the instruction.
Valid = any float
X1
REAL
array
X-axis array, table one. Combine with the Y-axis array, table one to define the points of the first piece-wise linear curve.
Valid = any float
Y1
REAL
array
Y-axis array, table one. Combine with the X-axis array, table one to define the points of the first piece-wise linear curve.
Valid = any float
X2
REAL
array
(optional)
X-axis array, table two. Combine with the Y-axis array, table two to define the points of the second piece-wise linear curve.
Valid = any float
Y2
REAL
array
(optional)
Y-axis array, table two. Combine with the X-axis array, table two to define the points of the second piece-wise linear curve.
Valid = any float
FUNCTION_GENERATOR Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true.
In
REAL
The analog signal input to the instruction.
Valid = any float
Default = 0.0
XY1Size
DINT
Number of points in the piece-wise linear curve to use from table one. If the value is less than one and Select is cleared, the instruction sets the appropriate bit in Status and the output is not changed.
Valid = 1 to (smallest of X1 and Y1 array sizes)
Default = 1
XY2Size
DINT
Number of points in the piece-wise linear curve to use from table two. If the value is less than one and Select is set, the instruction sets the appropriate bit in Status and the output is not changed.
Valid = 0 to (smallest of X2 and Y2 array sizes)
Default = 0
Select
BOOL
This input determines which table to use. When cleared, the instruction uses table one; when set, the instruction uses table two.
Default is cleared.
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled. Cleared to false on overflow
Out
REAL
Output of the instruction.
Status
DINT
Status of the function block. By default, the Style is HEX.
InstructFault (Status.0)
BOOL
Instruction generated a fault.
XY1SizeInv (Status.1)
BOOL
Size of table 1 is invalid or not compatible with the array size.
XY2SizeInv (Status.2)
BOOL
Size of table 2 is invalid or not compatible with the array size.
XisOutofOrder (Status.3)
BOOL
The X parameters are not sorted.
Description
The following illustration shows how the FGEN instruction converts a twelve-segment curve.
FGEN Graph
The X-axis parameters must follow the relationship:
X[1] < X[2] < X[3] < ... < X[XY<n>Size],
where XY<n>Size > 1 and is a number of points in the piece-wise linear curve and where n is 1 or 2 for the table selected. You must create sorted X-axis elements in the X arrays.
The Select input determines which table to use for the instruction. When the instruction is executing on one table, you can modify the values in the other table. Change the state of Select to execute with the other table.
Before calculating Out, the X axis parameters are scanned. If they are not sorted in ascending order, the appropriate bit in Status is set and Out remains unchanged. Also, if XY1Size or XY2Size is invalid, the instruction sets the appropriate bit in Status and leaves Out unchanged.
The instruction uses this algorithm to calculate Out based on In:
  • When In Less than or equal to X[1], set Out = Y[1]
  • When In > X[XY<n>Size], set Out = Y[XY<n>Size]
  • When X[n] < In Less than or equal to X[n+1], calculate Out = ((Y[n+1]-Yn)/ (X[n+1]-Xn))*(In-Xn)+Yn
Affects Math Status Flags
No
Major/Minor Fault
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition
Function Block Action
Prescan
Rung-condition-out is cleared to false.
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in.
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in.
Execute FGEN algorithm.
Postscan
Rung-condition-out is cleared to false.
Examples
Example 1
In this example, the FGEN instruction characterizes a flow signal which is then totalized using a TOT instruction. The FGEN_01X1 and FGEN_01Y1 arrays are REAL arrays of 10 elements each to support up to a 9 segment curve. You can use arrays of any size to support a curve of any desired number of segments.
Ladder Diagram
FTDS FGEN LD example 1.png
Example 2
This example passes optional parameters to FGEN instruction.
Ladder Diagram
FTDS FGEN LD example 2.png
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal