View status

Create a backing tag for the FGEN instruction.
  1. On the instruction, select Configure icon.
    The
    FGEN Properties
    dialog box opens.
  2. In
    Status
    , view the read-only status information for blocks containing status bits.
    If no status bits are set,
    OK
    displays. Otherwise, the parameter names associated with the set status bits appear, typically indicating which parameters have invalid values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal