Configure FGEN

Prerequisites
  • Create a backing tag for the FGEN instruction.
Changes made in the
FGEN Properties
dialog box are committed immediately:
  • Offline
    . Each change is committed to the DSL. Invalid entries are accepted, and validation errors are reported in the DSL.
  • Online
    . Each change is committed to the controller. Invalid entries are rejected, and an error dialog box reports the issue.
To configure FGEN
  1. On the instruction, select Configure icon.
    The
    FGEN Properties
    dialog box opens.
  2. On
    General
    , do the following:
    • Tag Name
      . View or change the tag name.
    • Description
      . Enter an optional description.
  3. On
    X, Y Arrays
    , do the following:
    • Table 1
      . Select the tags for X1 Array and Y1 Array.
    • Table 2 (Optional)
      . Select the tags for X2 Array and Y2 Array.
    TIP: The arrays for each table must be at least as large as the displayed value for
    Table 1 - # elements required
    and
    Table 2 - # elements required
    . These values are controlled by the
    XY1Size
    and
    XY2Size
    parameters respectively.
  4. On
    Parameters
    , update the values for the listed parameters as needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal