Work with phases
You can command various phases in the batch from the Procedure view. The following commands can be applied to phases from either the SFC or Table view:
Start
, Hold
, Restart
, Abort
, Stop
, Reset
, Pause
, Resume
, Comment
, Manual
, Semi-Auto
, Auto
, Clear Failures
, Bind
, Release
, and Disconnect
. These commands only affect the selected phase.Provide Feedback