Manual phase control binding

Each manual phase control session begins when you select an equipment module from within a unit. The materials that can be manipulated are a function of the container associations on that equipment module.
The dialog box prompting you to enter the Batch ID now includes the selection of a
material - container - use
.
ePro_client_MBR_Manual_Phase_Control
When you select a line in this dialog box, you are selecting the material to be used, the storage container to bind the equipment module with and whether a material addition or distribution is to be made. This enables the AMOUNT parameter to be prompted and its range checked to see that the value entered suits an addition or distribution phase.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal