Off-line material binding

If the Material Server is unavailable to provide material data, you can continue to run material-based recipes in
eProcedure
. The area model and the recipe provide most of the information, which leaves only the information about actual materials and lots unknown.
When the Material Server is unavailable (off-line), you are prompted to select a unit, even when the binding type is
First Available
. Notice in the following illustration that the
Capacity
column contains a 0 value, while the
EU
,
Lot
, and
Label
columns are blank.
ePro_MBR Material Phase Prompt to Bind dialog
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal