Reactivate an instruction

Reactivate past instructions in a phase that is currently RUNNING that does not have pending, reactivated steps. Reactivate one instruction at a time. If the
Reactivate
command was configured with a signature template in
FactoryTalk Batch Equipment Editor
, the signature request displays in the instruction being reactivated.
Prerequisites
  • If
    Past
    instructions do not appear in the
    Prompts
    list, select the box to the right of the
    Filter
    bar, and clear
    Hide Past
    .
  • Ensure property security privileges for the step to reactivate.
To reactivate an instruction
:
  1. Select a valid past instruction, and then select
    Reactivate
    .
  2. Change any incorrect values.
  3. If a signature request displays, enter the required User ID and password, and a comment, if required, and then select
    Sign
    .
  4. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal