Add devices
Opening a controller in FactoryTalk Design Studio opens a tab for the controller, shows an overview of the controller, and displays views to configure settings for the controller. The devices have these views to configure:
- Overview
- Port configuration
- Time synchronization
Action buttons on the pages write changes to settings on a page:
- OK. Write any changes to settings on the current page to the controller and close the controller tab.
- Apply. Write any changes to settings on the current page to the controller and leave the page open.
- Cancel. Close the controller tab without saving any changes to settings on the current page.
- Help. Display user assistance for the current view.
Provide Feedback