Time Synchronization view
How do I open Time Synchronization view?
- On the explorerbar, select
Devices. - InDevices, right-click the controller and selectOpen.
- In the device profile, selectTime Synchronization.
Use
Time Synchronization
view to view time synchronization status and enable or disable time synchronization on the controller. Enabling time synchronization allows the controller to participate as a clock in the system time. It also allows the controller to become a master clock for the system or to become a master clock in the chassis.If the controller is the grandmaster clock, all devices connected to the controller synchronize with the clock of the controller.
Time Synchronization
view displays details for the device that is acting as the grandmaster clock.Provide Feedback