Overview view
How do I open Overview view?
- On the explorerbar, select
Devices. - InDevices, right-click the controller and selectOpen.
- In the device profile, selectOverview.
Use
Overview
view to display the definition of a controller. Information in Overview
view includes the device name and type, revision, electronic keying, and the position of the controller in the chassis. Provide Feedback