Points view (output devices)

Use the
Points
view to:
  • View a summary of the points for the output devices.
  • Configure the behavior of each output point when:
    • a communication fault occurs and the device enters Fault mode.
    • the controller transitions to Program mode. While in Program mode, outputs from the controller are ignored, and the output behaves according to the behavior selected.
    • a communication failure occurs while the controller is in Program mode.
  • For some of these output devices, configure additional parameters and diagnose a problem with an output point.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal