Configure points for an output device

Configure point properties for the output devices.
To configure the points for an output device
  1. On the tab for the device, select
    Points
    .
  2. In the
    Points
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal