Diagnose a problem with an output point
Diagnose these counter problems from the
Points
view:- Whether a short circuit fault exists.
- Whether a no load fault exists.
Diagnostics is disabled when:
- You are operating offline.
- An Identity mismatch exists.
To diagnose a problem with an output point
- On the tab for the device, selectPoints.
- In thePointsview, in theDiagnosticscolumn for the point, select
.
Provide Feedback