HART Command view

Use the
HART Command
view to automatically configure the HART Field Device with user supplied PV Damping and Range values.
When these features are enabled, the device sends the PV Damping and PV Range values to the HART Field Device connected to the channel.
TIP:
To make the
HART Command
view available, go to
Device definition
, and then configure these two parameters as:
  • Input Data
    = Analog and HART by Channel
  • Configure HART Device(s)
    = Yes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal