Select the units for the PV range
Use
Select PV Units
to select PV units
for the PV Upper Range
and Lower Range
values.Prerequisites
- Make sure that these two parameters inDevice definitionare set to correct values:
- Input Data= Analog and HART by Channel
- Configure HART Device(s)= Yes
To select the units for the PV range
- On the tab for the device, expandChannels, and then expand an individual channel.
- SelectHART Command.
- In theHART Commandview, select (...).
- InSelect PV Units, specify these parameters:
- CategoryCategory of the unit, such as power, electrical, and temperature. If there is no suitable category,Enter ID Valueis assigned.
- PV UnitsUnit of measure associated with the category. Not available whenCategoryis set toEnter ID Value.
- PV Units IDUnit ID associated with the unit. WhenCategoryisEnter ID Value, a value between 1 and 255 is assigned. The default is 32.
- SelectOKto confirm and save the changes.
Provide Feedback