HART Command view parameters

The
HART Command
view includes these parameters.
Parameter
Description
Enable HART Device PV Damping Configuration (Command 34)
Indicates that the HART Field Device is automatically configured using the value entered in
PV Damping
. The device sends Command 34 to the Field Device connected to the channel when the device is connected.
PV Damping
is not available when this checkbox is cleared.
PV Damping
Indicates the PV Damping value for the HART Field Device.
Enable HART Device PV Range Configuration (Command 35, Command 47)
Use the values entered in
PV Units
,
PV Upper Range
,
PV Lower Range
, and
PV Transfer Function
to configure the HART Field Device.
When the checkbox is cleared,
PV Units
,
PV Upper Range
,
PV Lower Range
, and
PV Transfer Function
are not available.
PV Units
Indicates the units for the
PV Upper Range
and
PV Lower Range
.
Browse
(
...
) opens a dialog box for selecting the units for the PV range.
PV Upper Range
The
PV Upper Range
value must be greater than the
PV Lower Range
value.
PV Lower Range
The
PV Lower Range
value must be less than the
PV Upper Range
value.
PV Transfer Function
Indicates the transfer function used between the Loop Current and Primary Variable's digital value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal