ChX view (output devices)

Use the
ChX
view to:
  • Select the output range and current or voltage mode
  • Enable HART communications
  • Configure the sensor offset
  • Select to hold for initialization
  • Scale the signal to engineering units
  • Select the output behavior in Program mode
  • Select the output behavior in Fault mode
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal