Alarms view parameters
The
Alarms
view includes these parameters:Parameter | Description |
---|---|
Disable All Alarms | Disables all alarms for a channel. Not configurable when in Run mode. |
Process Alarming | Sets the maximum and minimum values for the process alarms using the settings in the individual channel view for High Engineering and Low Engineering .The alarm thresholds are in engineering units, but they can lie outside the Low Engineering and High Engineering. If the alarm thresholds lie outside the range of the input device, the alarm checking feature is turned off. Refer to MSG service codes for additional information. Process Alarming settings cannot be configured when in Run mode.Requirements:
|
Latch Process Alarms | Maintains the process alarm even after the condition ceases. The alarm only unlatches with an explicit message acknowledging the alarm. Not configurable when in Run mode. |
| The level of input to a channel that causes the device to set the Ch x HHAlarm indicator bit. The alarm remains active until the input returns below this level, by more than the deadband. If Latch Process Alarms is selected, the Chx HHAlarm indicator bit remains set until explicitly cleared. |
| The level of input to the channel that causes the device to set the Ch x HAlarm indicator bit. The alarm remains until the input returns below this level, by more than the deadband. If Latch Process Alarms is selected, the Chx HAlarm indicator remains set until explicitly cleared. |
| The level of input to the channel that causes the device to set the Ch x LAlarm indicator bit. The alarm remains until the input returns above this level, more than the deadband. If Latch Process Alarms is selected, the Chx LAlarm indicator bit remains set until explicitly cleared. |
| The level of input to the channel that causes the device to set the Ch x LLAlarm indicator bit. The alarm remains until the input returns above this level, more than the deadband. If Latch Process Alarms is selected, the Chx LLAlarm indicator bit remains set until explicitly cleared. |
Deadband | The value where an alarm, once set, remains available as long as the input value is within the deadband range of the alarm trigger point. (This value in combination with the process alarms creates the range.) This prevents the alarm from cycling on and off if the process value hovers near the alarm threshold. Deadband must be less than half the distance between the Low Limit value and the High Limit value.Deadband is not configurable when in Run mode.Refer to Example of Deadband configurations for additional information. |
Enable Rate Alarm latching | Maintains the rate alarm even after the condition ceases. The alarm only unlatches with an explicit message acknowledging the alarm. Not configurable when in Run mode. |
Rate Alarm Limit | The maximum ramp rate value that triggers a Rate Alarm when the Input Signal rate of change exceeds the setpoint. This alarm is in engineering units/second. This is useful for detecting rapid process changes. Valid range is 0 ≤ Rate Alarm Limit ≤ 100,000,000. If 0, Rate Alarm Limit is disabled.Not configurable when in Run mode. |
Unlatch | Unlatches the adjacent alarm condition. Not available when offline. Unlatching can be performed when in Run mode. |
Unlatch All | Unlatches all alarms for the channel. Not available when offline. Unlatching can be performed when in Run mode. |
Provide Feedback