Example of Deadband configurations

These images show typical Deadband configurations. Specifically the images show the Deadband at its limit for the given High and Low alarm settings. The Deadband is over the limit if the red and blue bands overlap.
HART_Alarms_WTUDC_capture01
HART_Alarms_WTUDC_capture02
The Deadband must be less than half the distance between the Low alarm and High alarm.
RSLogix 5000
software shows the deadband with red and blue shaded areas.
HART_Deadband
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal