WebTrend Migration Tool

Use the WebTrend Migration Tool to migrate
FactoryTalk® VantagePoint®
trends to WebTrend. This tool applies to
FactoryTalk VantagePoint
version 8.00.00 and later. You must have administrator privilege on the
FactoryTalk VantagePoint
server and WebTrend server.
IMPORTANT:
  • While the Asset framework and Data Archive are connected to the WebTrend server, if the tags of a
    FactoryTalk VantagePoint
    trend are not bound to the Asset Framework and Data Archive, these tags will not be displayed on the canvas when the trend is imported to WebTrend.
  • For the trend tags from the Asset Framework, this tool will identify the Data Archive where the tags are bound. Therefore, if tags from multiple Asset Framework databases are bound to the same Data Archive tag, only one Asset Framework tag can be imported to WebTrend.
  • WebTrend version 1.00.00 only supports
    FactoryTalk® Historian Site Edition
    as the data source.
Rockwell Automation®
recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal