Export trends from FactoryTalk VantagePoint

To export trends from
FactoryTalk VantagePoint
  1. Go to
    <FactoryTalk Historian SE installation package>\Redist\OtherComponents
    .
  2. Copy
    MigrationTool.zip
    into the
    FactoryTalk VantagePoint
    server computer and extract
    MigrationTool.zip
    to the desktop.
    TIP: The user signing in to the
    FactoryTalk VantagePoint
    server must have administrator permission to access the
    FactoryTalk VantagePoint
    database.
  3. In the
    MigrationTool
    folder, double-click
    WebTrendMigrationTool.exe
    .
  4. On the
    WebTrend Migration Tool
    page, select the tab.
    Ensure that
    FactoryTalk VantagePoint
    is running.
  5. Enter the
    FactoryTalk VantagePoint
    database instance name.
    Find this name in
    VantagePoint Manager
    >
    Configuration
    >
    IncuityStore Database
    >
    Server
    .
  6. Select
    Load trends
    .
    All trends from
    FactoryTalk VantagePoint
    are listed in the table.
  7. Select the trends that you want to export, and then select
    Export as JSON
    .
    WebTrend does not allow duplicate trend names.
  8. In the
    MigrationTool
    folder, choose a folder to save the exported JSON file.
  9. Once the export is completed, click
    target folder
    to find the JSON file and relevant logs.
    We do not recommend modifying this JSON file, because it may corrupt the file format and cause the migration to fail.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal