Set up the sample demonstrations
The installation process places the
SampleDemo1
and
SampleDemo2
folders in the FTBatch_Projects share on the batch server
machine. Each of these SampleDemo
folders contains four subfolders with the
files for the sample application, including the area model and recipes.- To run the sample demonstrations:
- Configure the Network Editor to locate the material database.
- Add aFactoryTalkSecurity user.
- Configure theFactoryTalk BatchServer to locate the area model.
- Verify the recipes in the area model.IMPORTANT: The default databases MaterialBasedRecipe and SAMPLE2_Materials cannot be removed from SQL Server. You are free to add another database and use it for production or test, but you must keep the originally installed databases intact even though they are not being used.
Provide Feedback